AXIS#.IL.KPLOOKUP

Description

The keyword can take 0 or 1 arguments. With no arguments the keyword prints the entire 256 element gain scheduling table. With one argument, it prints the table value at the specified index.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read

Units

%

Range

0 to 255

Data Type

Float

See Also

AXIS#.IL.KP

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.